8/27/2010 12:18 PM | |
Posts: 12 Rating:
|
Thank you for reply J_Bell I have detail question for you. The S7-200 must be connected with the S7-300 master using Fiber Obtics Profibus cable. so which module is need to add to S7-200 station and S7-300 station? Best Regards |
8/27/2010 4:49 PM | |
Posts: 5822 Rating:
|
Dear hcn, as you do PROFIBUS and you want to create an optical ring topology the OLM PROFIBUS is the choice I would choose. |
This contribution was helpful to
1 thankful Users |
Follow us on