10/4/2023 7:04 AM | |
Joined: 7/19/2022 Last visit: 4/23/2025 Posts: 436 Rating:
|
Hello Gorobets, You must also load the project on the panel in addition to the CPU. If you have a backup loaded on the panel and you do not have the original project, you should not change tag names, IP addresses... because communication between the CPU and the panel will be lost. |
If this Information really helps, you could use the Rate function |
|
10/4/2023 7:51 AM | |
Joined: 5/15/2018 Last visit: 10/30/2024 Posts: 23 Rating:
|
Its interesting. I will try now and write the result... |
Follow us on