3/2/2012 11:34 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Some questions in return How is connection made between panel and CPU ? According to attached manual there are 2 options.(chapter 5) Are there some settings in the panel like refresh-rate or update cycle time? Maybe there is the problem? Regards, Marcjan Attachmentgt-connect-other-company-plcs-manual-f449e-8-0911.pdf (82 Downloads) |
Problem solved? |
|
3/3/2012 2:03 AM | |
Posts: 1 Rating: (0) |
Dear Sir, Thank you for your reply. We used PPI Cable with RS 232 connection. And we used option 1 from your drawing (we have drawing too and I Attached). We already check and set on the panel (Cycle time, bautrate and etc) but the result is same. But, when we use the other PLC (LG PLC) all is normal condition. Thanks, BR Nur AttachmentPLC-Software-LG-gt-other-plcs.pdf (75 Downloads) |