6/7/2011 9:22 AM | |
Posts: 3 Rating:
|
Hi there , i have the same problem with an s7-200 cpu 224 ... can you tell me if you have solve that problem please ? i have upload a picture here . Thank you
|
6/14/2011 12:34 PM | |
Joined: 4/22/2010 Last visit: 12/15/2022 Posts: 5697 Rating:
|
Then there must be something terrible wrong with the wiring of the port or the level of the signals is to high. Attached the pin assignment of the S7-200 communication port, notice that there is 24V on the same connector, maybe you shortwire these pins. Best regards, Marcjan Attachmentspin-assignments.pdf (134 Downloads) |
Last edited by: Marcjan at: 6/14/2011 12:36 PMProblem solved? |
|
6/14/2011 1:05 PM | |
Posts: 3 Rating:
|
Thank youMarcjanfor your support , i have double checked all the wireing and everithing looks OK . i guess that the only thing that remains is the grounding . Best regards.
|
Follow us on