5/19/2010 9:45 AM | |
Posts: 2930 Rating:
|
Hi, here some examples: Via SMS: http://support.automation.siemens.com/WW/view/en/21063345 Via GPRS: http://support.automation.siemens.com/WW/view/en/39099329 The second one can be changed. Publish the HTML-Pages on the PC back to Internet (Port 80) via MWSL script. Advantage with MWSL scrip: On the mobile devicesno SW must be installed and each Browser is supported (WinCE, Opera, ......) I have seen tests at Hannover fair 2009 at the Siemens boot, working with PDA, MDA, mobile phones (Siemens, Nokia, Sony, i-Phone, Samsung, Sagem, ....). Any mobile unit with access to Internet was able to display the HTML-Page. I hope this helsp |
5/19/2010 11:46 AM | |
Joined: 2/5/2009 Last visit: 9/14/2023 Posts: 36 Rating:
|
Tanks Helmut |
Follow us on