1/11/2016 7:28 AM | |
Posts: 7 Rating: (0) |
Hello, I've a problem with S7-200 PLC connected to a machine, this problem occurred when i dismounted the PLC to show it to a trainers .When i constracted the PLC again, the PLC stop and machine became stop !. So that i've redownload the application to the PLC again via Micro/WIN but the PLC stay not responding !. I'd like to mention that the battery in the battery cartridge is low and i don't sure if the battery status might cause such a problem?.. Help me please..Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/11/2016 10:39:33 AMNew subject after splitting |
|
1/12/2016 9:27 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on