7/31/2012 1:49 PM | |
Posts: 163 Rating:
|
Respected sir/mam, I have two s7 300 CPUs --->(1) 314C-2DP and (2) 315C-2DP and both are interfaced with CP 343-1 lean for data exchange between them. There is ethernet switch between two CPs and one HMI is also connected to that switch which is to be communicated with 1st CPU. Please check the system architecture which is attached. Can you please tell me wether it is possible to communicate with HMI and transfer data between two CPUs........ Please reply me as early as possible............................ regards Attachmentsystem-architecture.zip (52 Downloads) |
Last edited by: rudrani at: 8/1/2012 7:20 AM |
|
7/31/2012 1:54 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Dear rudrani, No attachment found!!!! |
VANDE MATARAM..... |
|
8/5/2012 11:03 AM | |
Posts: 163 Rating:
|
please reply me on my thread....... regards, Rudrani
|
8/5/2012 11:06 AM | |
Posts: 163 Rating:
|
Respected sir/mam, Please reply me for my question of system architecture....... Regards, Rudrani
|
8/5/2012 11:08 AM | |
Posts: 1064 Rating:
|
Yes you can with the setup you have . |
8/6/2012 7:27 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
How to exchange the data between two Cp343-1 Lean - in attachment example based on ISO on TCP conncetion. Best regards, Hristo Mihalev
AttachmentTCP IP Sample S7-300.zip (59 Downloads) |
Follow us on