8/12/2015 10:47 PM | |
Joined: 5/9/2011 Last visit: 10/16/2024 Posts: 71 Rating:
|
Hi Maria, I will give you the quick answer; first of all it should be possible to access your PLC through the internet. Having Port 102 open is a good start, however did you configure port forwarding in your router? Once you have forwarded the Port you need to find out what the "internet" IP address of your PLC is. In your local network example 192.168.1.50 is what your IP might look like, however if you try to access your network through the internet and a router you will find that another IP is assigned. When you are on a computer that is on the same IP as your PLC use google and type in "what is my IP?" This is the IP address that you will need to assign in your SCADA application. In the local network of your PLC you need to go into your router and forward the port of this PLC to your router to make it accessible through the internet. When you access your router you need to forward the local IP address to your router. When you configure the SCADA you should only need the IP of the PLC , the same IP you need to download the program to the PLC, the CP will do its job without any extra configuration. Just remember that the IP to access the PLC locally is not the same as when going through the internet and you will need to do port forwarding in your router. Rgds Another even simpler way to access a remote network is by using Teamviewer VPN, have a look at the attached PDF. This way you are connected to the other network via Teamviewer and it is just as good as being on the same network. You can also find another post on the Teamviewer setup here. AttachmentHow%20to%20setup%20Teamviewer%20VPN.pdf (101 Downloads) |
Last edited by: Bosbreker at: 8/13/2015 10:40:41 AM |
|
Follow us on