1/7/2011 7:41 AM | |
Joined: 4/21/2006 Last visit: 1/27/2025 Posts: 510 Rating:
|
Hi evilofddc22, please write in English. Thanks. Blue Moderator |
This contribution was helpful to
3 thankful Users |
1/7/2011 12:17 PM | |
Joined: 4/21/2006 Last visit: 1/27/2025 Posts: 510 Rating:
|
Hi Muthamizh Selvan, please write also in English (or additional in English). Blue Moderator |
1/7/2011 2:00 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Maybe a short summary for everyone. evilofddc22 has an AS-i CP with address 256..271. He does not see the relation between this address and the AS-i slaves and how to address the individual inputs and outputs in the S7 program. In my opinion, the answer to this is in this manual: http://support.automation.siemens.com/WW/view/en/5581657 in chapter 4, as of page 39, depending type of slave used (address in range A, Address in range B, and so on...). The manual is also available in french at this link http://support.automation.siemens.com/WW/view/en/5581657/0/fr Clickingon the icon "Info" (floppy) you can downlaod a sample program. |
Best regards |
|
This contribution was helpful to
2 thankful Users |
1/7/2011 8:49 PM | |
Posts: 3 Rating:
|
Thanks for your help I find the Organisation Block wich AsI inpout and output are read and write . |
Follow us on