12/20/2010 6:14 AM | |
Posts: 111 Rating:
|
I have the same problem, specially in writing codes in PLC in order to get data from slaves. |
12/20/2010 2:34 PM | |
Joined: 9/27/2006 Last visit: 3/19/2025 Posts: 12344 Rating:
|
Hello Siemens_user_1; The functions SFB P_SND_RKand SFB P_RCV_RK are the heart of the Modbus master communications, using the CP 341. The datab;locks IDB_xxx_xxx are the instance DBs required to have the SND_ and RCV_ blocks work properly. Please review the sample applivcation program included in the Modbus Master manual, so you can understand how these fuctions and blocks work together to establish Modbus communications with a CP 341 (or a CP 441-2); see the attached document for an illustration. http://support.automation.siemens.com/WW/view/en/1220184 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/20/2010 3:41 PM |
|
Follow us on