7/26/2009 8:46 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Vijay, This kind of DO is possible to detect wire break even when the output signal is "0". And I think, depending from electrical connection is possible to receive SF when disconect wires from fuses. Of course you should enable in hardware configuration wire break diagnostic. You could read more about diagnostic for this type of DO in follow link - SM322-8BH01 Digital Output Module with Diagnostics. Hope this will helps. Best regards, Hristo Mihalev |
7/28/2009 2:58 PM | |
Posts: 101 Rating: (0) |
Dear UMENCHO & IBN-SERVICE Thank you Regards, Vijay |
Follow us on