5/4/2012 6:34 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, please see the FAQ. Which memory cards can you use with a S7-300 CPU? you will get all the details as required.
For that you need to haveoriginal offline program available with you all the time.
Sorry to Say that but you need atleast wiring Details for IO. With that Details you need to add all this IO in Symbol Table Manually. If not then it is really difficult to understand logic. |
Last edited by: Amit_86 at: 5/4/2012 7:46 AMsee Fritz reply for second question Last edited by: Amit_86 at: 5/4/2012 6:42 AMVANDE MATARAM..... |
|
5/4/2012 7:10 AM | |
Joined: 10/7/2005 Last visit: 9/10/2024 Posts: 3020 Rating: (1054)
|
it is actually possible, but requires additional download of the zipped up S7 project and you'll find all the details on how to do so in the FAQ's below: How can you load projects to a memory card and back again to a PG/PC? How can you also store other files that belong to the project or plant on the MC/MMC? How do you save a STEP 7 project as read-protected on an MMC in an S7-300 CPU? S7-300: How can I find out the size of the MCC so I can store my whole STEP 7 project on it? I hope this helps |
Cheers |
|
This contribution was helpful to3 thankful Users |
5/4/2012 11:36 AM | |
Posts: 14 Rating: (2) |
This answered very clear & thanks for all |
This contribution was helpful to1 thankful Users |
Follow us on