3/1/2012 6:17 PM | |
Joined: 4/22/2010 Last visit: 2/26/2025 Posts: 5697 Rating:
|
Hello, Few things to check. Number of hmi connections in the CPU settings. Mpi adress off the CP (if you have one) and panel not the same? See attachment page 2 what i mean. If possible, make some screenshots of your hardware config, so whe can find your problem. regards, Marcjan Attachmentconnection.pdf (303 Downloads) |
Last edited by: Marcjan at: 3/1/2012 6:20 PMProblem solved? |
|
This contribution was helpful to
1 thankful Users |
3/1/2012 6:48 PM | |
Joined: 1/26/2012 Last visit: 2/17/2022 Posts: 11 Rating:
|
Tomorrow I will make some screens. CPU have MPI address 2, CP module MPI address 3 (i have only one CP module). In GP panel i set MPI address 2 and the same transfer speed like in CPU. I loading screens to GP via Ethernet but communicate with PLC via MPI directly (without adapter). Generaly everything is working its mean communication GP<->PLC is working properly but in the same time is not working communication PC<->CPU I found something inhttps://support.automation.siemens.com/WW/llisapi.dll/23643456?func=ll&objId=23643456&objAction=csView&nodeid0=18308132&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=contentin point 8.3 that the communication can be aborted
|
Last edited by: maciekelga at: 3/1/2012 7:42 PMLast edited by: maciekelga at: 3/1/2012 6:56 PM |
|
3/3/2012 10:38 PM | |
Joined: 1/26/2012 Last visit: 2/17/2022 Posts: 11 Rating:
|
When I change settings MPI address another than 2 GP is not working, it`s freeze after reset is the same. When MPI is 2 (the same like in CPU) then is working ok, only i can`t start monitoring in Step7, but Ethernet connection with S7-1200 is working properly. Generaly everything is ok, only is not working connection PC- S7-300 via Ethernet (it`s not possible to turn on monitoring). In attachments screens my hardware settings: Attachmentscreens.zip (239 Downloads) |
3/5/2012 10:15 PM | |
Joined: 1/26/2012 Last visit: 2/17/2022 Posts: 11 Rating:
|
I have same settings like in attachment, when I changed PG and OP to 2 still was same problem like before. |
Follow us on