2/8/2017 8:02 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hello, can you try to upload in HWConfig? Regards Christoph |
2/8/2017 8:12 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Dear Sir, I have tried to upload in HW Config but still the same error. I have managed to get the backup of this project when i try to open the project it displays the below error. I have seen the vfd number and firmware from the back up project and installed the gsd in my software. |
Thanks |
|
2/8/2017 8:22 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
I have searched for PROTOOL software but seems it is discontinued and the replacement is WINCC FLEXIBLE 2008 sp2 which i am currently downloading and installing. But is the PROTOOL the actual problem for the g120 not appaering in the hardware configuration. |
Last edited by: Satheesh290692 at: 2/8/2017 8:26:33 AMThanks |
|
2/8/2017 8:23 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hi, this message means that the project contains a ProTool HMI Device and the SW is not installed on the system. And which VFD with which FW?
Christoph |
2/8/2017 8:48 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Dear Sir, How can I find whether the software is installed in Starter OM ? I have attached the details of the g120 drive below. |
Thanks |
|
2/8/2017 9:07 AM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
Hi, if you can see the drives and open the properties then the correct OM is installed on the System.
Christoph |
2/8/2017 10:39 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
any other solution experts? |
Thanks |
|
2/14/2017 5:18 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
Dear All, I have sucessfully uploaded all the program without any error messages. cause: protool software missing solution: install WinCC Flexible 2008 sp3 Thanks |
Thanks |
|
2/14/2017 9:31 AM | |
Joined: 3/8/2011 Last visit: 5/17/2023 Posts: 262 Rating: (20) |
Hello Satheesh, Does missing drives connected on Profibus physically ??? |
If this post helped you, you may use the Rate-button |
|
2/15/2017 5:35 AM | |
Joined: 4/28/2015 Last visit: 4/12/2024 Posts: 112 Rating: (3) |
hello Dongerpure, YES, They are connected physically. |
Thanks |
|
2/15/2017 6:42 AM | |
Joined: 4/25/2011 Last visit: 2/15/2024 Posts: 40 Rating: (1) |
Hi Satheesh, I have some points please clarify me. 1.Do you have the old any project back up what you are trying to upload. 2.If Yes, then check whether it is going online or not. 3.Confirm me when you were downloaded the configuration last time, have you received any SDB error or interrupted in between while downloading. |
Nobody is Perfect and i am nobody....If it is helpful please Rate it. |
|
Follow us on