4/1/2019 12:51 AM | |
Joined: 6/4/2008 Last visit: 2/6/2023 Posts: 1418 Rating:
|
Hi all, it was us being daft. Instead of directly writing P2507=2 (and monitor for the change P2507=3) AND THEN setting P971=1 on the DO, which works fine, We were writing to the Homing block input signal "Set reference point" which really misleadingly changes the position actual value to whatever the home coordinate value you set in P2599 - but this DOES NOT save the calculated offset when you trigger P971=1 on the DO. Had this POST been somewhat better described in the subject, I would have found the correct sequence earlier - I was searching for strings like "absolute" "encoder" "offset" "RAM" "ROM" etc Regards, Graeme |
Follow us on