5/11/2012 4:28 PM | |
Posts: 559 Rating: (87) |
Dear ace_sinergize, That is OK. If you CPU A is master & IM of A has become faulty then redundancy system will switchover IM only but not the CPU. Why you want the CPU to change from Master to Slave? This system will work perfectly. There will not be any problem. AttachmentControl_Word_Status.pdf (230 Downloads) |
5/13/2012 3:32 AM | |||
Posts: 559 Rating: (87) |
Dear ace_sinergize, Thanks for your reply. Have you defined the parameters for FC 100 as per your actual hardware configuration? I am also attaching the file for your ready reference. Please go through it and define paramters for I/O & IM like PIO_FIRST, PIO_LAST, SLAVE_NO, SLAVE_LEN, SLAVE_DISTANCE once again & see the result. Always download the change in this parameter by deleting DB5 (Instance DB of FB 101 'SWR_ZYK') from the online CPU & after that you download change in the both the PLCs. AttachmentFC_100.pdf (196 Downloads) |
||
5/17/2012 8:04 PM | |
Posts: 559 Rating: (87) |
Dear ace_sinergize, Any update please? Please reply. |
Follow us on