2/2/2010 4:01 PM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308)
|
Hello Solution Riders, Did you install software redundancy package? I've extracted the following text fromsoftware redundancymanual. 1.5 The Library of Blocks for Redundant Software Backup When the optional software package is installed, the library SWR_LIB is created in STEP 7. You can access that library in SIMATIC Manager using the menu command File > Open > Libraries. The library SWR_LIB contains five block packages. Two are for S7-300 and three for S7-400. You use a specific package according to the type of connection and network via which the two stations are linked. |
Follow us on