6/2/2009 10:09 AM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
Hi automatinglego, I think it will too hard to test SWR with only two CPUs without IM 153-3(or IM 153-2 asPegaiasaid). Most of the SWR tricks appears during the HOT test nothing appears in the Simulation. So I recommend to have all the used products in hand the start your test till this you can read lots of threads in this forum concerning the problems of SWR. Best Regards |
Last edited by: Khaled_Ezzat at: 6/2/2009 10:17 AMBest Regards |
|
Follow us on