11/29/2007 9:50 AM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello Mike; Siemens has an applicationdocument where they suggest the INAT Echochange gateway (http://www.inat.de/):"Communication between SIMATIC S7 and Allen-Bradley ControlLogix CPUs via Ethernet: Use of "Echochange" gateways". Here is the link to the Application and Tools file: http://support.automation.siemens.com/WW/view/en/23901499 Here is a brief description of how the gateway operates: An Allen Bradley PLC wants to communicate with a Siemens PLC. ● Application data is encapsulated (CIP header). ● To encode CIP messages in Ethernet frames, the encapsulation header is added. ● TCP is used as transport protocol. A TCP header is added, then an IP header and lastly the MAC header. ● This Ethernet frame arrives at the echochange. ● Echochange has to convert TCP data with AB protocol into TCP data without application protocol. Therefore the MAC header, IP header, Encapsulation header and CIP header are removed. ● In accordance with the settings the data is encoded again and an RFC1006 header, TCP header, IP header and MAC header is added to the data. This Ethernet frame is transferred to the Siemens PLC. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 29.11.2007 09:51 |
|
10/23/2015 9:23 AM | |
Joined: 4/14/2010 Last visit: 2/8/2025 Posts: 525 Rating:
|
(http://www.inat.de/) Now this company is Permanently Closed any alternative..??? |
MS |
|
10/23/2015 3:13 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello Sarfraz; A possible solution has been presented by GJohn; see the attachment. You can find more information here: www.redlion.net/data-acquisition/data-station-plus Hope this helps, Daniel Chartier |
Follow us on