7/13/2011 2:18 PM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
Hello AnoopKP
anice overview of the differences can be found in the thread below: What differences exist in the 300-series Industrial Ethernet CPs?
It depends is the only answer I can give you. You would definetely need toknow the link config in the S5's CP143 tobe able to configure a corresponding link on the S7but may also need to change/adjust the CP143 configuration. Below is an ISO example link for your perusal and note the additional links in them too: Where can you find sample programs and documentation for communication from SIMATIC S5 modules to SIMATIC S7 modules via Industrial Ethernet using the ISO transport protocol? I hope this helps |
Cheers |
|
7/13/2011 2:55 PM | |
Joined: 4/24/2006 Last visit: 3/19/2025 Posts: 8903 Rating:
|
Dear AnoopKP, Have a look at this link: What differences exist in the 300-series Industrial Ethernet CPs?
Perhaps the following link might help: Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet Best regards, Wizard |
Follow us on