5/23/2011 8:39 PM | |
Joined: 6/7/2010 Last visit: 7/9/2024 Posts: 571 Rating:
|
Hello... Find the attached document.How to configure CPU, ET module & setting the IP address. MMC card is used to store your PLC data. AttachmentCPU & ET module interface.zip (245 Downloads) |
Regards, |
|
5/24/2011 8:19 AM | |
Joined: 10/22/2008 Last visit: 2/17/2025 Posts: 372 Rating:
|
So the et200PN is with its own CPU and can handle logic? I can ommit s7-300 CPU and control with et200? |
5/24/2011 9:59 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Yes, you could use FB 14/15 (GET/PUT) in order to exchange data between CP343-1 Lean and PN CPU. Make a S7 connection in PN CPU side and CP343-1 Lean will be a passive parther. And yes, CPU PN supports T-blocks... Which communication services are supported by CPUs with an integrated PN interface? Best regards, Hristo Mihalev |
5/24/2011 10:18 AM | |
Posts: 947 Rating:
|
Hi May be this link help you: Comunnication with profinet between cpu 314 with cp lean and ET200S CPU: /tf/WW/en/Posts/56158 |
Follow us on