10/23/2015 10:42 AM | |
Posts: 31 Rating:
|
Hi, You could use open source communication using OPC scout or Kepware. |
10/26/2015 1:45 PM | |
Posts: 160 Rating:
|
Please, take a look at the doc. (I do not know what do you mean by "communication Oracle and Siemens CPU"). Janko Attachment470690 - Open Sockets Support in ControlLogix and CompactLogix systems.pdf (146 Downloads) |
10/26/2015 1:52 PM | |
Joined: 9/27/2006 Last visit: 3/23/2025 Posts: 12344 Rating:
|
Hello Muhammad; Please see if the answer provided in this thread is sufficient for your needs:
Communiction ORACLE with PLC - Service - Siemens There are more threads on this subject in the forum, search for them using the Search Box at the top right of this page. Hope thius helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
10/26/2015 3:03 PM | |
Joined: 4/14/2010 Last visit: 2/8/2025 Posts: 525 Rating:
|
Thanks dchartier, According to above link please confirm. Only included in 6GK1704-1CW13-0AA0 SIMATIC NET Which One is Suitable 6GK1704-1CW13-0AA0 SIMATIC NET OR KepWare..?? 2. Is CPU 317-2 PN/DP Sufficient for Oracle Data Base Communication OR any other required..?? There are 05 Allen Bradley compact logix CPU and One PC which have Oracle Data Base all are parallel in hub switch on Ethernet/IP application Layer. Want to Communicate with>>>>>
another SIEMENS System which is separate with S7-300 PN/DP + WINCC PC in connectivity of Industrial Ethernet/ISO through CP1612. as we know (if i wrong please correct me) Both having different layer and can't Talk directly>>> For the OPC communication should we use one gateway for the conversion of Ethernet/IP AB PLC to Industrial Ethernet/ISO Siemens PLC..??? Regard's |
MS |
|
Follow us on