7/12/2010 1:05 PM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
Which SIMATIC S7-300/S7-400 modules support the NTP time-of-day message and how do you activate this kind of time synchronization? |
7/14/2010 8:16 AM | |
Posts: 12 Rating:
|
Tomorrow I will be at the customer again and will check with diagnostics (did not know that would work with PN) what's going on. |
7/14/2010 5:15 PM | |
Posts: 5822 Rating:
|
Hello, personally I fear you will not see in the NCM special diagnostics if the PN CPU updates the time by the NTP server. The only device you would be able to check about this would be the CP, this is right... and I think this is what you thought, don't you? |
7/16/2010 12:06 PM | |
Posts: 12 Rating:
|
I tried to perform some diagnostics using NCM but this seems not possible. NCM says "No diagnostics possible for the module with module ID 6ES7 318-3EL00-0AB0". I did not find any other way to check the server connection, not in the Module Information en not in Hardware Diagnostics. Actual status: A windows XP machine is capable of synchronizing the time of day with another windows XP machine which serves as time server. Although the settings in the CPU / PN appear to becorrect and linked to the IP address of this time serverno time synchronization takes place. There seems no apparantway of diagnostics. I'm out of options, any help much appreciated. |
Last edited by: flynowworklater at: 7/16/2010 12:06 PM |
|
7/16/2010 2:06 PM | |
Posts: 5822 Rating:
|
Hello, I know these questions may sound a bit strange... but I need to ask them. J_Bell |
7/16/2010 2:21 PM | |
Posts: 12 Rating:
|
Ok, I'll dig further into this, but first I go on holiday. Thanks so far and I'll let you know the outcome (in a few weeks from now). |
8/9/2010 4:51 PM | |
Posts: 12 Rating:
|
Reading about stratum I understand your remark now. However I fail to see the relevance (becauseof a complete lack of understanding I presume). |
Follow us on