5/7/2015 3:35 PM | |
Posts: 3 Rating:
|
Problem with the Y-Link that is necessary to read approximately 1 Kbytes of data. You will need 4 or 5 pieces Y-Link! I would like to avoid it. |
5/8/2015 3:04 AM | |
Joined: 10/7/2005 Last visit: 3/15/2025 Posts: 3042 Rating:
|
Hello karriandr I fear you are out of the luck. In order to make the IE/PB link directly available for both CPU's of a H system it must support so called "Profinet System Redundancy" (which the IE/PB unfortunately does NOT support). You could still physically connect and use it as part of your S7-400H Profinet network, BUT it only be used as one-sided I/O's (i.e. it belongs to only one of the H CPU's and if that CPU goes down, the IE/PB link is also lost to the partner CPU, have a look too at https://support.industry.siemens.com/tf/us/en/posts/s7-400h-with-third-party-device-on-profinet/107727 for more on this). One can only hope that a new IE/PB link that supports Profinet System Redundancy (as well as MRP) is in development and will come out one day soon (may be worth your while to check directly with Siemens). Until such time though, good old Y-Link and Profibus is the way to go for you. I hope this helps
|
Last edited by: fritz at: 5/8/2015 5:46:53 AMfixed up corrupted formatting Cheers |
|
This contribution was helpful to
2 thankful Users |
5/8/2015 3:22 PM | |
Posts: 3 Rating:
|
Hi. fritz! It's all clear now. Many thanks for the clarification! |
This contribution was helpful to
1 thankful Users |
9/27/2017 7:55 AM | |
Joined: 6/14/2006 Last visit: 2/20/2025 Posts: 301 Rating:
|
Hi, I only know about PCS 7 environment. There is the IE/PB-Link PN IO. The IE/PB LINK PN IO is a gateway between Industrial Ethernet and PROFIBUS. It enables seamless integration of PROFIBUS devices in the PROFINET fieldbus. The IE/PB LINK PN IO acts as a proxy: i.e. from the viewpoint of the IO controller, the integrated DP slaves are handled like IO devices with Ethernet interface. See chapter 3.7 of https://support.industry.siemens.com/cs/attachments/72887082/72887082_PCS7_PROFINET_Blueprints_DOC_en.pdf Regards |
9/27/2017 4:09 PM | |
Joined: 11/18/2010 Last visit: 3/12/2025 Posts: 2 Rating:
|
Thank you Myst This document helped me a lot. |
Follow us on