5/26/2014 12:32 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating:
|
Hi! Yes, it is possible to make fault-tolerant H-connection via TCP/IP (ISO on TCP) with 416-5H CPU. For more information, lookthismanual, and then specify your question more detailed. Hope it helps. |
This contribution was helpful to
1 thankful Users |
5/28/2014 10:53 AM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating:
|
HiPPPD With Simatic Net V8.1+SP2 you will need a CP1623. With Simatic Net V8.2 and WinCC V7.2 you can also use Redconnect via ISO on TCP with a normal ethernet adapter
|
Best Regards |
|
5/28/2014 11:25 AM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
How do you configure a fault-tolerant S7 connection for the SIMATIC NET OPC server via Industrial Ethernet with the SIMATIC NET PC software? |
5/28/2014 12:04 PM | |||||||||||
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating:
|
In addition toUMENCHO The below FAQ shows an important settings for setting up thefault-tolerant S7 connections over ISO-on-TCP
|
||||||||||
Best Regards |
|||||||||||
This contribution was helpful to
1 thankful Users |
5/29/2014 7:46 AM | |
Posts: 63 Rating:
|
After doing all necessary steps, in case of any trouble do check services for redundancy. Goto start menu and type "services.msc" in search or run tab |
5/30/2014 6:15 AM | |
Joined: 3/21/2006 Last visit: 3/14/2025 Posts: 10239 Rating:
|
Yes, it will work with the new 400H. Best regards, Hristo Mihalev
|
This contribution was helpful to
2 thankful Users |
5/30/2014 9:56 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating:
|
Apparently this will work according to below thread: /tf/WW/en/Posts/85580 |
This contribution was helpful to
1 thankful Users |
Follow us on