6/8/2011 10:59 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, Use a DP/DP Coupler. There you will need two. Look at an old dicussions regards same issue. 1. S400H & DP-DP Coupler 2. DP DP coupler on S7 400H system Best regards, Hristo Mihalev |
This contribution was helpful to
2 thankful Users |
6/9/2011 7:27 AM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
I think Y-Link supports S7-400 like a slave there. Look there Using a CPU as I-Slave at the Y link only during deactivated mode "Commissioning/Test operation" Best regards, Hristo Mihalev |
This contribution was helpful to
2 thankful Users |
6/9/2011 7:30 AM | |
Joined: 10/7/2005 Last visit: 3/24/2025 Posts: 3042 Rating:
|
Hello Vispute Prashant You can have a CPU as an I-Slave downstream of a Y-Link, but must in this case do a GSD file based configuration. Have a look at the link below for more on how to configure it: Configuring an S7 CPU as DP slave on the H system using a Y-Link |
Cheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on