3/6/2015 5:04 PM | |
Joined: 5/12/2006 Last visit: 3/14/2025 Posts: 22588 Rating:
|
Hi,
yes this should be no problem. |
This contribution was helpful to
1 thankful Users |
12/22/2019 2:31 PM | |
Joined: 8/30/2016 Last visit: 10/24/2022 Posts: 5 Rating:
|
PLCS71500 and S7300 can communicate together via CP343_1. Based on the S7 connection, you can communicate. However, you have to ensure the CP343_1 must support the ethernet connection if the version of CP343_ is too old, it not support the connection, then you have to change this module. Goold luck. Attachments7communication_s7-1200_s7-300_en.pdf (977 Downloads) |
Follow us on