1/8/2014 1:59 PM | |
Posts: 1368 Rating: (126) |
Hello Mohammad, do you connect the IM154s only with one CPU412-3H? Is it possible to post your hardware configuration? Thx, Pittiplatsch |
1/11/2014 8:37 AM | |
Posts: 44 Rating: (4) |
Hello, I got it from Hardware configuration online (Module information / communication tab), see attached. Regards, Mohammad
|
1/11/2014 8:38 AM | |
Posts: 44 Rating: (4) |
also the same for the other CPU (see attached) Regards, Mohammad
|
1/28/2014 9:15 AM | |
Joined: 8/19/2013 Last visit: 3/6/2024 Posts: 148 Rating: (10) |
Hello Mohammad Abu- we do not have your complete configuration but i guess there are some other services that allocate S7-ressources. Means on each S7-connection thatyou have created in Netpro is 1 S7- ressource but other services also use S7-ressources therefore the total amount is 12. Please have a look to the following http://support.automation.siemens.com/WW/view/en/44444467 Chapter 4.2 commuication services Hope this clarify that a little bit Regards |