7/9/2013 10:34 AM | |
Joined: 1/3/2012 Last visit: 2/26/2024 Posts: 17 Rating: (0) |
Dear TEBANCH, Thanks alot. Please find the attached pic. |
Last edited by: mahmoud.abualrub at: 7/9/2013 10:34 AM |
|
7/9/2013 12:49 PM | |
Joined: 1/3/2012 Last visit: 2/26/2024 Posts: 17 Rating: (0) |
Hello TEBANCH, Really this is first time for using this modules, where i can found F block?? thank you |
7/9/2013 3:07 PM | |
Joined: 3/25/2008 Last visit: 1/28/2022 Posts: 232 Rating: (20) |
Hello, well first a brief description of Fail Safe vs "Normal" CPU's can be found in many threads, i suggest yot to take a look to some of them . A fail safe aplication requieres special hardware (FCPU's as well as FIO modules), from you hardware configuration i see that you have both, also you will need "special" software S7 F configuration pack (i guess you have it, because it is no posible to compile HW configuraton for FCPU's with out this option). Having said that, an F block (FC or FB)is a logic block but created by means of FLAD editor (which is included in the S7 F config pack), in F aplicationsif you have an FDO module (as per say your SM326) you are not allowed to write to those outputs in a "normal" FC or FB, you shall write those in an F-FB or F-FC. Well i thing is time to you continue your research, if you have more questions please let us know. Plase Review some FAQs. Regards. |
Keep working! |
|
This contribution was helpful to1 thankful Users |
7/9/2013 5:22 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello mahmoud, Download the Following Manual & try to Configure as per that, SIMATIC Industrial Software S7 Distributed Safety - configuring and programming Product Information to the manual, Edition 01/2010 S7-300 Distributed I/O device ET 200 M - Fail-safe signal modules From Above Module you will come to know the Basic of the F System Configuration & Program... |
Ammy |
|
4/25/2016 9:03 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by sina20795 is split to a separate thread with the subject Diagnostic feature s7 417-5H. Best regards |
Follow us on