12/1/2010 2:59 PM | |
Posts: 70 Rating:
|
Hi I avoid Global Data for time critical functions. Use the internal ports e.g. the MPI in a small local network and configure them as profibus with three partisipants. Make S7 connection in netpro and use e.g. Put functions from the owner of the IO. (or BSEND) Please see this thread where I have shared some gained expirience Søren |
12/3/2010 5:15 PM | |
Posts: 5822 Rating:
|
Hello, I am sorry, but I would recommend useing this way: S7 Communication via K bus with the S7-400 MPI is by far not as fast as the K-Bus. Best regards J_Bell |
Follow us on