6/26/2008 1:50 PM | |
Posts: 487 Rating:
|
Well, the answer is right there in your question. You are telling you used VIPA CPU as 315-2DP. That should be the problem. You can not replace a slave type with something else. Master can detect that, even if the IO areais thesame. What you need to do is, get the GSD file for VIPA CPU as slave and install the GSD in Step7 HW catalog. Here is the link for download http://www.vipa.de/en/service/downloads/gsd-files/ Then use this toconfigure your slave Hope this info will help you to fix the problem. |
6/27/2008 1:36 PM | |
Posts: 487 Rating:
|
Good to know you solved the problem |
Follow us on