9/30/2021 5:55 AM | |
Joined: 12/18/2014 Last visit: 5/27/2024 Posts: 33109 Rating: (4087) |
S7-PLCSIM Advanced V4.0 - Correction of the V3.0 API versionExchange of the V3.0 API files with the V3.0 Update 2 files within the S7-PLCSIM Advanced V4.0 S7-PLCSIM Advanced also delivers the older API interfaces with any released version. In V4.0 these are V1.0, V2.0, and V3.0. Customers who e.g. want to communicate with a SIMIT V10.2 or V10.3 Update 1 with the S7-PLCSIM Advanced in bus-synchronous mode should use the following instructions. To ensure trouble-free operation, the API files must be exchanged with those from this article. As soon as S7-PLCSIM Advanced is installed in a higher version than 4.0 (e.g. V4.0 UPD1 etc.), this behavior is corrected by the setup automatically. |