4/19/2013 4:05 PM | |
Posts: 1547 Rating:
|
Hello, to connect a s7 PLC from non windows os you can use a native TCP-Conection, or if required an udp connection. Fro this you must use the FC5 and FC6 block on PLC. A sample you will find here: How do you program the communication blocks FC5 and FC6? It is suggested to use fixed data length, hae a look to this FAQ: Behavior of the communication processors during data transfer via TCP connections without RFC 1006 |
Follow us on