11/14/2017 9:40 AM | |
Joined: 8/25/2014 Last visit: 2/3/2023 Posts: 10 Rating:
|
I've opened the request yesterday, hope that we can find the correct fix. The support guy told me that there is this simple guide to follow: https://support.industry.siemens.com/cs/ww/it/view/75164975 But unfortunatly for me i've only have the SDA standard compliant SD Host controller driver and no other compatible hardware ( i've also tried to install every driver not compatible for the SD card reader, none is working). If i reinstall windows from the Restore DVD that came with the package of the M4 after the restore is finished i find only the "SDA standard compliant SD Host controller driver" no other hardware as showed in the upper Link. The support also told me that they will send my information to siemens in germany. I will inform on this post to let also other user resolve their problem. |
Last edited by: Jen_Moderator at: 11/15/2017 2:52:12 PMInserted right link |
|
This contribution was helpful to
2 thankful Users |
Follow us on