12/26/2009 6:10 PM | |
Posts: 1 Rating: (0) |
isnt it possible to communicate s71200 and Wincc 7.0 ?? i can ping to my plc but wincc says no connection to the plc.. |
12/26/2009 7:44 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, If I refer to this link: http://support.automation.siemens.com/WW/view/en/38051469 it seems not possible to do it directly. |
Last edited by: edr at: 12/26/2009 7:45 PMBest regards |
|
12/28/2009 11:05 AM | |
Joined: 9/23/2005 Last visit: 1/15/2025 Posts: 4393 Rating: (1463)
|
Hi, once it is possible to connect S7-1200 with SIMATICNET using OPC interface, ( http://support.automation.siemens.com/WW/view/en/39960680) you can use this interface to connect WinCC to S7-1200 |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
12/29/2009 2:06 PM | |
Joined: 11/29/2009 Last visit: 1/13/2025 Posts: 19 Rating: (0) |
Hi! When we connect the WinCC to S7-1200, can we use this (sendind and receiving information)through TCP? |
4/20/2010 8:18 AM | |
Posts: 26 Rating: (4) |
Hello, I can access all links... glubb |
4/21/2010 10:31 PM | |
Posts: 37 Rating: (2) |
Thanks Pegaia for your usual support and cooperation. glubb , please follow the attached PDF that explain how to set up the OPC “step-by-step”. Once you configure the OPC, try to configure the WinCC as in the attached screenshot. I have tested, working okay.. Cheers AttachmentS71200.zip (1534 Downloads) |
This contribution was helpful to1 thankful Users |
9/20/2014 9:28 AM | |
Joined: 1/14/2013 Last visit: 6/30/2024 Posts: 2 Rating: (1) |
Hey MANS, Thanks for the attachment sent.. It helped a lot.. Nitin |
Follow us on