5/30/2019 10:23 AM | |
Joined: 12/17/2013 Last visit: 6/3/2022 Posts: 41 Rating:
|
Dear all, i followed the topic as i am trying to figured out the proper setup and choose the appropriate hardware. In my case i want to use a Sick incremental encoder (see Attached) with electrical interface 7..30 VDC, TTL/RS422. I am confused regarding the output signal of the Encoder, as i knew the output signal of the encoder is independant of the power supply to it (regarding this type of signal out), so i thought i will need the sb 6ES7221-3AD30-0XB but i see that huggy_d1 in a topic
also suggests the 24VDC version of it. How is this going to work? i mean what i am missing?? Thank you in advance AttachmentDBV50E-22CKA2000_1079596.pdf (142 Downloads) |
Follow us on