10/28/2015 1:47 PM | |
Joined: 7/9/2015 Last visit: 3/18/2025 Posts: 4200 Rating:
|
Hi tmdawc,
a S7 1214c DC/DC/DC can do 16 connection maximum and will support S7 Communication. You should compare your PLC with the Data Sheet your the PLC. Example: S7-1200 CPU 1214C DC/DC/DC https://support.industry.siemens.com/cs/de/en/pv/6AG1214-1AG40-4XB0/td
Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
3/14/2018 4:29 PM | |
Posts: 2826 Rating:
|
Hello.
Why are you not using the built-in Ethernet port? Does that module handle S7 communications?
BR |
This contribution was helpful to
2 thankful Users |
3/15/2018 10:55 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, as is described in manual, no problem with S7 communication. |
With best regards... |
|
3/15/2018 11:00 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, did you enable the PUT/GET-communication in HW-config of the S7-1200 PLCs? regards, |
FCK WAR! |
|
Follow us on