Industry Online Support
Technical Forum
1/19/2009 5:12 PM | |
Posts: 34 Rating: (0) |
Dear Sir Can TP177A or TP177Bcommunicate with two numbers of S7200 - CPU226 which configured as a master and slave cpu on MPI network. If yes please find the attached program screens and guide me any changes in the configuration. ( Another configurationScreen) Thanks and regards Muthukrishnan A&D-CCR Coimbatore Attachmentwincc_screen.zip (98 Downloads) |
1/20/2009 12:38 AM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question posted more than once. The thread which got replies is published with the subjectS7200 and TP177B or TP177A communication withinthe conference SIMATIC Panel. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on