3/11/2009 3:20 PM | |
Joined: 3/21/2006 Last visit: 1/14/2025 Posts: 10239 Rating: (1182) |
Hello Look at this FAQ: How can you communicate data between the S7-200 and the S7-300 via PROFIBUS DP? Hope this will helps. regards |
Last edited by: UMENCHO at: 3/11/2009 3:26 PMOuops! Forgot the example for MPI connection. http://support.automation.siemens.com/WW/view/en/747743 Last edited by: UMENCHO at: 3/11/2009 3:24 PMIf you don''''''''t want to buy EM277, you can use MPI connection between both CPU. Be careful, MPI connection has restrictions in speed, distance between both CPU, quontity of data which will be exchange. |
|
3/14/2009 2:30 PM | |
Posts: 3 Rating: (0) |
Thanks so much, but i am still searching for the functions and programming blocks... and for a sample project as too if it exist Regards, Alverz |
3/14/2009 2:32 PM | |
Posts: 3 Rating: (0) |
Thanks so much, but i am still searching for the functions and programming blocks... and for a sample project as too if it exist Regards, Alverz |
Follow us on