1/14/2011 3:12 PM | |
Joined: 10/7/2005 Last visit: 11/28/2023 Posts: 2996 Rating:
|
Hello Info1 only the S7-400 has a two channel CP441-2 serial interface module avilable but going down this path would be cost prohibitive. The best advise I can give you is to consider using an ET200S IM151-7 CPU with 4 off 1SI serial interface modules (6ES7138-4DF01-0AB0). I haven't done the costing of it but you will hopefully find that this is the most cost and space efficient solution. I hope this helps |
Cheers |
|
1/14/2011 3:17 PM | |
Joined: 8/31/2005 Last visit: 11/24/2023 Posts: 2196 Rating:
|
Did you notice the ET200S modules? Maybe a ET200S station with this modules is a solution for you. |
|
|
1/20/2011 12:05 AM | |
Joined: 7/2/2008 Last visit: 11/27/2023 Posts: 928 Rating:
|
Hello Info1, Are you sure the ET200S will take more space?!! S7-300: 1*CPU (4cm) + 4* serial interfaces (16cm) +1*AI (4cm) + 1*AQ(4cm) + 1*DQ (4cm). This will give you a total width of 32cm ET200S: CPU (6cm) + 1* Power module (1.5cm) + 4*serial interfaces (6cm) + 4*AI (6cm) + 1*AQ (1.5cm) + 2*DQ (3cm). This will give you a total width of 24cm. Best regards. H-H |
2/24/2011 5:31 AM | |
Joined: 8/31/2006 Last visit: 8/18/2023 Posts: 4 Rating:
|
Maybe ,you can use like this RS322C->RS485 andthen use one cp341(RS485) |
5/5/2011 2:28 PM | |
Posts: 17 Rating:
|
Been doing alot of research on this at the moment, why not use the CP341 expansion card and communicate to the devices via RS485? or are the devices all RS232? |
Follow us on