4/2/2019 3:27 PM | |
Posts: 17 Rating:
|
Hello Everyone, I am facing an issue with the basic functionality of the Modbus RTU communication blocks for ET200SP CM ptp module (6ES7 137-6AA00-0BA0) with S7-400H I am trying to establish master RTU communication using the FB640 (modbus_comm_load) and FB641 (modbus_master)... when enabling the REQ for FB640 (modbus_comm_load) I am receiving the DONE bit and The following STATUS = 7000... so I assume this block is working fine. after that I enable the REQ for FB641 (Modbus_Master) and only receive the BUSY bit and the following STATUS = 7001 , which means Block is "Initial call after request started". and this is not a very helpful status. the modbus device information i am trying to access is as follows : Baudrate: 19200
So please if anyone has any idea how to resolve this , I would appreciate it thank you Cheers! AttachmentCM_PTP_ISSUE.zip (194 Downloads) |
4/2/2019 5:54 PM | |
Posts: 3093 Rating:
|
Hello, How do you evaluate the status of system blocks in STEP 7 (TIA Portal)? Regards, |
Follow us on