2/16/2010 9:37 AM | |
Joined: 3/14/2008 Last visit: 7/11/2025 Posts: 2203 Rating:
|
@ Mods: Don't know if this must be a new subject... AttachmentVLT5000.zip (253 Downloads) |
Last edited by: Blue Moderator at: 16.02.2010 10:02splitted and renamed from this: /tf/WW/de/Posts/39548#top If I could help you, you can use the RATE button. Thank you. |
|
2/16/2010 12:18 PM | |
Joined: 3/14/2008 Last visit: 7/11/2025 Posts: 2203 Rating:
|
Hello Daga, I'm gonna try your method! The drives are going to work with PID control and other loops and will not only be used for start/stop/reset. The drives are integrated into pcs7, 21 of them. I'll post the results.. Thxxx |
If I could help you, you can use the RATE button. Thank you. |
|
2/16/2010 12:36 PM | |
Joined: 3/14/2008 Last visit: 7/11/2025 Posts: 2203 Rating:
|
Hmm ok, I thought i needed to use these blocks because I'm sending and recieving data with more than 4 bytes.. As for the Process image, If I click the input/output modules that are in my drive, I see that the process image isn't selected. It's grey, so I can't select anything. The only thing i can find in the cpu is : update OB1 cyclically which is checked... |
If I could help you, you can use the RATE button. Thank you. |
|
2/16/2010 1:16 PM | |
Joined: 3/18/2009 Last visit: 12/6/2024 Posts: 306 Rating:
|
What is the MLFB of your CPU? |
2/16/2010 1:24 PM | |
Joined: 3/14/2008 Last visit: 7/11/2025 Posts: 2203 Rating:
|
6ES7416-2XK00-0AB0 CPU416-2DP built until '98 Extra information: CPU is in a plant, ten years old and was operated under pcs7 4.0. The drives are connected at profibus master 2: IM467 module. Currently, i made a testproject in simatic with a simple db/fc.. my system is pcs7 7.1 And yeah the cpu need to be replaced...to be compatible with 7.1. |
If I could help you, you can use the RATE button. Thank you. |
|
2/17/2010 8:14 AM | |
Joined: 3/14/2008 Last visit: 7/11/2025 Posts: 2203 Rating:
|
Dear daga, |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on