1/21/2008 4:44 AM | |
Posts: 27 Rating: (2) |
I am using Safety Matrix Engineering Tool V5.2 After creating the martix in the tool i am using Tool--> Transfer to Project When the transfer takes place the chart is generated in the Chart folder of same name, but in the chart the Channel Driver is Not automatically generated. Only Locked @Matrixname chart is generated. After compilation of the chart following error is generated. E: Parameter WHP_C+E_MATRIX\\PRO_WELLHEAD_1\@PRO_WELLHEAD_1.C1.Tag2_B_4 is not interconnected with a data source (block output, global address) AttachmentWHP_SSDS_Compile.zip (135 Downloads) |
Last edited by: smulekar at: 21.01.2008 04:45 |
|
1/29/2008 4:05 AM | |
Posts: 27 Rating: (2) |
Hi All, I found the problem that the MatrixCAUSE inputin the CFC must be connected some where. So when i connected all the i/os of the Matrix Generated blocks there is no such kind of error. Now my problem is the Matrix Stops executing when i makeit on line with the PLC. Any one knows why matrix Stops Executing. I have attached the MATRIX CME.Connect all the I/O some where and try. AttachmentPRO_WELLHEAD_1.zip (154 Downloads) |
1/29/2008 4:08 AM | |
Posts: 27 Rating: (2) |
Hi KAs, I dont know that blocks whats the use of those. Also now i have no problem for transfer and compilaton error. |
1/31/2008 7:00 PM | |
Posts: 2661 Rating: (279) |
I tried with your matrix and it works fine. See attachment. What exactly is the error you are getting? What do you mean by "the matrix stops executing"? AttachmentSM_Online.zip (156 Downloads) |
Follow us on