12/1/2020 11:05 AM | |
Joined: 10/10/2018 Last visit: 3/26/2025 Posts: 6 Rating:
|
Dear all, I am trying to show the name of data records when I am using the event "ImportDataRecords" and request to overwrite the data record. But the name that appears is "Data record + number" (example: Data record 6). I use the event "SaveDataRecord" to save the name of data records and it works fine. But I think the name that appears is the "display name", so maybe I need to save the display name or make the name and the display name the same. It is possible? - Which TIA Portal Version do you use? (Version, Servicepack, Update) V15.1 - Do you use WinCC Basic/Comfort/Advanced Runtime or WinCC Professional Runtime or WinCC Unified (PC Based or Panel Based)? WinCC Advanced - Which Panel or Panel PC or PC (Version of Operating System)do you use? 6AV7230-0CA30-2CA0 - Windows 10 Enterprise 2016 LTSB - Create a clear Screenshot of the Problem if its Possible, because a Picture tells you more than 1000 Words Any suggestions will be appreciate. Thank you! AttachmentImages.zip (55 Downloads) |
Follow us on