1/13/2023 1:48 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
Where is the SD card insert? In the PC or in the LOGO!? |
1/13/2023 3:23 PM | |
Joined: 1/12/2023 Last visit: 1/13/2023 Posts: 4 Rating:
|
In the PC I try to transfer the program from the PC to the Logo |
1/13/2023 4:34 PM | |
Joined: 1/12/2023 Last visit: 1/13/2023 Posts: 4 Rating:
|
I dont get any info window. The card is 2gb and is formatted to 32bit. I am woundering if there is someting with the program but I installed it from the disc I got from the starter kit 6ED1057-3BA03-0AA8. AttachmentCar-O-Tronic Cable test 230111.zip (180 Downloads) |
1/13/2023 4:39 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
The info window tells you the problem: You have two blocks with open outputs. |
1/13/2023 4:42 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
Use open connectors to close the outputs of the two blocks. |
1/13/2023 4:45 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
And here the bin file of your program. The name of the file is "LOGO_U_P.bin". This is the only name that LSC and LOGO! accepted. AttachmentLOGO_U_P.zip (185 Downloads) |
1/13/2023 5:09 PM | |
Joined: 12/18/2014 Last visit: 12/1/2023 Posts: 31530 Rating:
|
Down in the right corner you can open the info window with a click on the symbol if the symbol appears. |
Follow us on