12/29/2017 8:50 AM | |
Joined: 4/28/2015 Last visit: 3/27/2025 Posts: 70 Rating:
|
Hello for all! I have a question about tegprefix technology in WinCC RT Prof V14.1. I created subscreen with his tagprefix (according to example TagPrefix example TIA v14). But now i need to save in the file csv all tags from my subscreen in depend of the current tag prefix. For example: I made the struct 'FAN" that contains tags: "SetTemp, SetSpeed ". On subscreen i have Iofields connected to " .SetTemp" and " .SetSpeed" respectively . I have several FANS. Now, when i open this subscreen in my main screen i can see value in IoFields depend of "tagprefix" .SetTemp and "tagprefix" .SetTSpeed. But i need to write or read in / from file the current value of the connected tag. I made buttons on subscreen with vb scripts for read/write data in /from file: Is it right syntax for this task? This code dosn't work For write in file
For reading from file:
|
Last edited by: hadok at: 12/29/2017 8:52:56 AM |
|
Follow us on