11/29/2014 8:33 PM | |
Posts: 6 Rating:
|
ThanksWilliam B.For Considering my post . I have Done what i want with FeildWrite . Now i am stuck in another Problem i want to Save values of Data block in Different data Blocks Using Hmi Ktp600 . It will be very help full for me if some one guide me proper direction . Asim Siddiq. ----------------- New subject after Splitting from How To Move Desire Array Element With Out Using Compare Function |
Last edited by: CS Moderator at: 11/30/2014 11:02 PMsplitting |
|
11/30/2014 7:32 AM | |
Posts: 6 Rating:
|
William B. yes it is like Recipe Control , The scenerio is that : There is Eight functions in plc program , and in each recipe these function calling in different sequnece with different values . Some of them functions, Calling more than one time in same recipe and having diferent values. For this I am using Data blocks in Plc to save recipes . There is 70 steps in one recipe so i am using 70 buttons at screen to Save values in 70 steps. Similarly using 70 bool tags in plc program which is much complicated . After saving that values in Data Block1 for First Recipe . Now i have to switch on Data block 2 For second Recipe. How can i switch ? Its becoming more complicated than my thinking If you guide me Best direction for this , Then It will be easy for me to achieve that Task.
|
11/30/2014 7:42 AM | |
Posts: 5225 Rating:
|
Hi there. This sounds very complicated. It is not a recipe in the tradisional sense. Recipes contain values (time, count, distance ++) not so much repeats of actions. Okay let us take it slowly.. Do I undertand correctly - you have 8 actions that can be repeated in various ways? .. |
11/30/2014 8:14 AM | |
Posts: 5225 Rating:
|
.. This is by no means a full program - but it may have enough clues on what start with on the PLC side. Please see the attached JPEG. w |
12/1/2014 5:39 PM | |
Posts: 5225 Rating:
|
Siddiq Asim, You can try the attached TIA11 project as a design idea for the HMI side. Note that the HMI project uses internal variables, so it will be possible to simulate the project without difficulty. There are two HMI pages. On the 1st page are 5 buttons. The description on each button can be changed by pressing on the button and navigating to the 2nd page. There the value of the button can be changed by making a selection. The consept of multiplexing is used. This same idea can be used inside the PLC instead of the internal variables. Chew on this a bit.. it might help. w AttachmentDesign idea_Multiplexing on KTP600.zip (176 Downloads) |
12/2/2014 10:09 AM | |
Joined: 9/1/2005 Last visit: 8/24/2023 Posts: 4099 Rating:
|
follow up question published by Parasis split to a seperate thread with the subject s71200 -working on a recipe . Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on