10/7/2015 4:30 PM | |
Posts: 439 Rating:
|
Hello DAutomatix, I would do that in your HMI. The segmented circular log overwritte the oldest entries when the maximum segment is written. So, I would use the segmented with a number of segments that fit your hour. You can then do a scheduled task every hour and use the event "ArchiveLogFile" and to move the log to your directory. You can use an HMI tag for the location. You can also do this with a VB script. Here is a link of an application example that use a script to create a folder to archive data: Long-Term Data Archiving with WinCC Runtime PC and SIMATIC HMI Operator Panels with WinCC (TIA Portal)Best regards, Hugo |
Last edited by: HugoD at: 10/7/2015 4:31:06 PMLast edited by: HugoD at: 10/7/2015 4:31:36 PM |
|
This contribution was helpful to
2 thankful Users |
Follow us on