10/13/2017 10:30 AM | |
Joined: 3/31/2015 Last visit: 4/25/2023 Posts: 175 Rating:
|
The IOP can store up to 16 fixed parameter sets and up to 235 parameter sets with customized names. Data sets are saved in ifs/config folder (fixed) but you can copy them to cps folder (custom) and rename them as you want using USB cable, PC and file explorer. You can save parameters from PC to IOP by simply copying them to the IOP using a USB cable (IOP works as mass storage device). I don't think you can export a *.bin file (parameter set) using TIA though. Please see the IOP manual for more info: https://support.industry.siemens.com/cs/document/109736312/ or IOP-2: https://support.industry.siemens.com/cs/document/109747658/ |
This contribution was helpful to
1 thankful Users |
Follow us on