12/5/2007 11:51 AM | |
Posts: 5822 Rating: (412)
|
Hello, I wonder, do you have a record made by Ethereal or Wiresharkt which you may post here? Best regards J_Bell |
12/5/2007 1:52 PM | |
Posts: 6 Rating: (0) |
Hello, Frame 1 (74 bytes on wire, 74 bytes captured) No. Time Source Destination Protocol Info Frame 2 (74 bytes on wire, 74 bytes captured) No. Time Source Destination Protocol Info Frame 3 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 4 (126 bytes on wire, 126 bytes captured) No. Time Source Destination Protocol Info Frame 5 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 6 (73 bytes on wire, 73 bytes captured) No. Time Source Destination Protocol Info Frame 7 (106 bytes on wire, 106 bytes captured) No. Time Source Destination Protocol Info Frame 8 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 9 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 10 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 11 (66 bytes on wire, 66 bytes captured) No. Time Source Destination Protocol Info Frame 12 (64 bytes on wire, 64 bytes captured)
Attachmentscalance_mailserver.zip (491 Downloads) |
12/7/2007 2:50 PM | |
Posts: 5822 Rating: (412)
|
Dear ToSo, I have to say that I do not get your Point. I usually use the Jana Server for such short tests, http://www.janaserver.de/ this one works great and is just one of many SMTP Severs available. The IT or Advanced CP is and will not becapableto use ID and Password to connect toa SMTP Server. Best regards J_Bell |
12/9/2007 6:18 AM | |
Posts: 6 Rating: (0) |
Good morning, I already stumbled across the janaserver, but for some reason I thought that wasn't the right thing. With your hint, I'll have a try... Regards Toso |
Follow us on